Technical FAQs

Ask a Question

What are the mounting options available for Compact NSXm circuit breakers.

Compact NSXm may be mounted vertically, horizontally or flat on their back or on their side without any derating of characteristics.
These devices can be mounted on a DIN rail using the integrated DIN rail mounting feature.
For backplate mounting, the devices are supplied with two mounting screws (M4),washers and nuts.
These mounting screws can be inserted through mounting holes molded into the device case and threaded into the mounting enclosure, rails or plate.





 
Was this helpful?
What can we do to improve the information ?