Technical FAQs

Ask a Question

RX/TX (10/100) LED indication is Off in NMC card AP9635 ?

Probable cause:
• The NMC is not receiving input power.
• The cable that connects the NMC to the network is disconnected or not functioning properly.
• The device that connects the NMC to the network is turned off or not operatingcorrectly.
• The NMC itself is not operating properly.                                                                                                                                                                                                                                                                                                   
Solution: It may need to be repaired or replaced.Contact APC by Schneider Electric Customer Support.
Was this helpful?
What can we do to improve the information ?