Technical FAQs

Ask a Question

Not able to access the user interface (UI) of NMC card AP9630?

Probable Cause & Solution:                                                                                                                                                                                                                                                                                                           
•Verify that HTTP or HTTPS access is enabled.
• Make sure you are specifying the correct URL — one that is consistent with the security system used by the NMC. SSL requires https, not http, at
the beginning of the URL.
• Verify that you can ping the NMC.
• Verify that you are using a Web browser supported for the NMC.
• If the NMC has just restarted and SSL security is being set up, the NMC may be generating a server certificate. The NMC can take up to one minute
to create this certificate, and the SSL server is not available during that time.

 
Was this helpful?
What can we do to improve the information ?