Technical FAQs

Ask a Question

How to Apply Power to PDU (PD60H5HK1)?

Follow the below steps to Apply Power to PDU (PD60H5HK1):

1. Close (turn ON) the main circuit breaker of the power source supplying power to the PDU.
2. Close (turn ON) the Main Input on the PDU.

3. Power the PDU distribution circuit breakers.
For PDUs with transformer:

a. Close (turn ON) the Main Output circuit breaker on the PDU.

Note: After the Main Output circuit breaker has been closed, both PDU distribution panels will be
energized.

For PDUs with and without a transformer:

b. Close (turn ON) the PDU distribution panel circuit breakers.

Note : When the distribution panel circuit breakers are closed, the PDU power cables
and connected equipment are energized.
Was this helpful?
What can we do to improve the information ?