Technical FAQs

Ask a Question

How to Ensure Total Power Off the PDU(PDRPPH1000)?

Follow the below steps to Ensure Total Power Off the PDU(PDRPPH1000)?

1. Open (turn OFF) the main breaker on the power source feeding the PDU.
2. Open (turn OFF) the Main Input switch on the PDU.
3. For PDU with transformer: Open (turn OFF) the Main Output circuit breaker on
the front of the PDU.
Was this helpful?
What can we do to improve the information ?