Technical FAQs

Ask a Question

How to Connect the InfraStruXure PDU(PDRPPH1000) to your network ?

Follow the below steps to Connect the InfraStruXure PDU(PDRPPH1000) to your network :

1. Connect a Cat-5 network cable to the surge-protected ethernet port on the PDU user connection
plate.
You can make connections from inside the enclosure, or you can remove the user connection plate
and make your connections.
Remove the plate using a Phillips or standard screwdriver to loosen
the two captive screws. Use the knockout in the plate to route cables to and from the user
connections on the plate. If you remove the plate, make sure that you do not disturb the existing connections.

2. Run the connected Cat-5 network cable through the knockout in the user connection plate to
your network connection.

3. Configure the TCP/IP settings of the InfraStruXure PDU.
Was this helpful?
What can we do to improve the information ?