Technical FAQs

Ask a Question

What are the TCP/IP configuration methods used to configure InfraStruXure PDU(PD60H5HK1) with your network?

TCP/IP configuration methods :

Use one of the following methods to define the TCP/IP settings needed by the InfraStruXure PDU:
ï  Device IP Configuration Wizard. 
ï  BOOTP or DHCP server. 
ï  Local computer. 
ï  Networked computer. 
Was this helpful?
What can we do to improve the information ?