Technical FAQs

Ask a Question

How do we configure InfraStruXure PDU(PD60H5HK1) through Device IP Configuration Wizard ?

Device IP Configuration Wizard:

You can use the Device IP Configuration Wizard on a Windows NTÆ 4.0, Windows 2000, or
Windows XP computer to discover unconfigured InfraStruXure PDUs and configure their basic
TCP/IP settings.

1. Insert the InfraStruXure PDU Utility CD into a computer on your network.
2. Launch the Wizard, when prompted, or, if prompted to restart the computer, access the Wizard
from the Start menu after the computer has restarted.
3. Wait for the Wizard to discover the first unconfigured InfraStruXure PDU, then follow the onscreen
instructions.

Note : If you leave the Start a Web browser when finished option enabled, you can use apc
for both the User Name and Password to access the InfraStruXure PDU through your
browser.
Was this helpful?
What can we do to improve the information ?