Technical FAQs

Ask a Question

How to connect InfraStruXure PDU(PDRPPH1000) using local computer ?

Local access to the control console :

You can use a local computer that connects to the InfraStruXure PDU through the console port on the
InfraStruXure PDU monitoring unit to access the control console.
1. Select a serial port at the local computer, and disable any service that uses that port.
2. Use the configuration cable (APC part number 940-0103) to connect the selected port to the
console port on the InfraStruXure PDU monitoring unit.
3. Run a terminal program (such as HyperTerminalÆ) on your computer and configure the selected
port for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control, and save the changes.
4. Press ENTER to display the User Name prompt.
5. Use apc for the User Name and Password.
Was this helpful?
What can we do to improve the information ?