Technical FAQs

Ask a Question

How to add a circuit breaker on the InfraStruXure PDU(PD60H5HK1) ?

Add a circuit breaker on the PDU :

1. Move the clip on the back of the circuit breaker to correspond to the phase to which you are connecting to (L1, L2, or L3).
2. Snap the new single-pole circuit breaker into a position on the panel.
3. Remove the corresponding plastic blanking plate on the front panel of the PDU.
Was this helpful?
What can we do to improve the information ?