Technical FAQs

Ask a Question

What is the purpose of holes shown in attached picture of BMXFTB2820 terminal block.




This area is for measuring purpose, all these terminals in this area are breakover with the every normal terminals 1-16 where cables are connected.

 
Was this helpful?
What can we do to improve the information ?