Technical FAQs

Ask a Question

What is the input resistance of analog output in ION7400.

The input resistance of analog output in ION7400 is as follows:

< 300 Ω (current mode)
> 500 kΩ (voltage mode)
Was this helpful?
What can we do to improve the information ?