Technical FAQs

Ask a Question

What is the maximum input voltage of digital output in ION7400.

The maximum input voltage of digital output in ION7400 is 30 V AC / 60 V DC.

 
Was this helpful?
What can we do to improve the information ?