Technical FAQs

Ask a Question

What is the maximum output voltage of digital output in ION7400.

The maximum output voltage of digital output in ION7400 is 250 V AC / 30 V DC.
Was this helpful?
What can we do to improve the information ?