Technical FAQs

Ask a Question

What is the Maximum output current of digital output in ION7400.

The Maximum output current of digital output in ION7400 is 8 A @ 250 V AC or 5 A @ 24 V DC, 20k cycles (resistive).
Was this helpful?
What can we do to improve the information ?