Technical FAQs

Ask a Question

If the C120H circuit breaker is locked ON with the 27145 padlocking facility will it still trip under fault conditions?

Yes, all of the miniature circuit breakers have a "trip free" mechanism which enables them to trip under fault conditions even if the handle is locked ON or held ON manually.

Was this helpful?
What can we do to improve the information ?