Technical FAQs

Ask a Question

What are the functions of LTMCU control operator unit

The LTMCU can be used to:

• configure parameters for the LTMR controller,
• display information about the LTMR controller configuration and operation,
• monitor detected faults and warnings detected by the controller,
• control the motor locally using the local control interface.
Was this helpful?
What can we do to improve the information ?