Technical FAQs

Ask a Question

What is the conformity to standards for LTMCU Control Operator unit.

The LTMCU conforms to IEC/EN 61131-2, UL60947-4-1A, CSA C22.2 no. 60947-4-1 standards.
Was this helpful?
What can we do to improve the information ?