Technical FAQs

Ask a Question

What is the resistance to shocks for LTMCU Control Operator unit.

The resistance to shocks according to IEC 60068-2-27 is Semi-sine mechanical shock impulse: 11 ms, 15 g on 3 axes.
Was this helpful?
What can we do to improve the information ?