Technical FAQs

Ask a Question

How XCKW wireless limit switch operates with ZBRRD receiver in Bistable Mode?

Receiver ZBRRD output goes logic HIGH once object push lever of XCKW and output remains high.
Once the object got removed and level get back to its normal position output of receiver goes to logic LOW.

Refer the below image:
 
Was this helpful?
What can we do to improve the information ?