Technical FAQs

Ask a Question

How XCKW wireless limit switch operates with ZBRRD / ZBRRC / ZBRN receiver in Monostable Mode?

Receiver ZBRRD output goes logic HIGH once object push lever of XCKW and output remains high for holding period. After Holding period it get back logic LOW

Once the object got removed and level get back to its normal position output of receiver goes to logic HIGH again for holding period. After Holding period it get back logic LOW.

Refer the below image:
Was this helpful?
What can we do to improve the information ?