Technical FAQs

Ask a Question

CRA and ERT Time Stamp modules Max Buffer Limit

Maximum number of I/O and available memory
 
BMX ERT 1604 T 16 discrete inputs on the module
255 events in internal buffer
BMX CRA 312 10 256 discrete I/O configured
4000 events in internal buffer
Was this helpful?
What can we do to improve the information ?