Technical FAQs

Ask a Question

How to update Advantys stb firmware

The procedure is automatically guided in the *.exe file in the link above. You just need to make the PC connected with STBNIP2212 via Ethernet and launch the exe. It will ask for the IP address after putting the IP address press enter it will automatically load the necessary file into the Module. Please make sure that during firmware upgrade STBNIP2212 module should not loose its power.

We have also attached the steps captured during firmware upgradation.

Firmware upgradation is not possible in running system and during firmware upgradation all the configuration/application/Initial values will be reseted. After completion of firmware upgradation IP address of NIm will be go to default(MAC address) and need to assign again.Configuration also need to download again.
Was this helpful?
What can we do to improve the information ?