Technical FAQs

Ask a Question

Altivar Process SEMI F47 settings

The design and dimensioning of the circuit makes Altivar Process Series drives possible to continue the operation in the limits that are stated in specification SEMI F47-0706 after setting of following parameters:

> Set "IPL" parameter to "NO" the phase loss function is de-activated.
> Adjust "uSL" parameter versus main supply value
> Adjust "uST" to upto 3s
> Set "STP" parameter to "MMS" DC bus maintained.

Refer the attached Manufacturer Declaration.
Was this helpful?
What can we do to improve the information ?