Technical FAQs

Ask a Question

How we can integrate Fipio devices using Momentum IO with Premium CPU.

170FNT11001 is a Fipio communication adapter to integrate FIP device to master controllers like premium. 

The 170 FNT 110 01 Fipio communicator establishes the interface between the Fipio bus, controlled by a Premium PLC and an input/output base from the Momentum product range. 
The communicator is compatible with all Momentum catalog connection bases. It can only be used when connected to a base.
 
Was this helpful?
What can we do to improve the information ?