Technical FAQs

Ask a Question

What factor should be considered for selecting toroids for Vigilohm fault detectors.

To select a suitable toroids, you need to consider about the cable size, installation environment.Then choose the toroids diameter size, closed or split toroids, if mild steel sleeve is needed.
 
Was this helpful?
What can we do to improve the information ?