Technical FAQs

Ask a Question

What is meaning of “N” at the end of a Harmony part number (example XB5AA42N).

The N at the end of a Harmony part number means that it is a local India offer sold and manufactured only in India. They aren't certified for the international market.
XB5AA42N and the XB5AA42 have the same function.
 
XB5AA42 is the standard product sold in the world wide.
XB5AA42N is dedicated for the local market India.
 
Was this helpful?
What can we do to improve the information ?