Technical FAQs

Ask a Question

what is rated operational current of ZBE101 for 440Vac.

Regarding ZBE101, in conformity with the IEC 947-5-1, if we are AC15 A600 we can mention other voltages:
 
380V: 1.9A
480V: 1.5A
500V: 1.4A
All of them are under constant power.
 
Thus, at operational voltage of 440VAC, the operational current of contact block ZBE101 will be 1.6A (approximately).

 
Was this helpful?
What can we do to improve the information ?