Technical FAQs

Ask a Question

Where can we find, information regarding the heat dissipation for ATV630 dv/dt output filter.

Here below the heat dissipation of the dv/dt filter:
VW3A5301: 16W
VW3A5302: 38W
VW3A5303: 49W
VW3A5304: 65W
VW3A5305: 92W
VW3A5306: 176W
VW3A5307: 287W

 
Was this helpful?
What can we do to improve the information ?