Technical FAQs

Ask a Question

Is digital encoder interface module VW3A3420 supports RS422/RS485 input signals.

VW3A3420 has three supply outputs:
+5V/250mA
+12V/100ma
+24V/100mA
It is mentioned on NHA8073000 Instruction sheet. please find in attachment.
VW3A3420 was designed, tested and is dedicated to support RS422/RS485 input signals only.

 
 
Was this helpful?
What can we do to improve the information ?