Technical FAQs

Ask a Question

What is the detection angle and range of CCT570003 detector.

  • Detection Angle ->120 ° to 360
  • Range -> up to 12 m
Was this helpful?
What can we do to improve the information ?