Technical FAQs

Ask a Question

In daisy chain network of Link150s, what is the distance between two Link 150 Device.

In link 150, 10/100 Base TX (802.3af) port standard is used for Link150 so maximum length is 100 meters.
Was this helpful?
What can we do to improve the information ?