Technical FAQs

Ask a Question

Which IP Rating enclosure should be used for contactor in high chemical environment.

When contactor are used in chemical environment we strongly recommend using IP6X protection enclosure or minimum IP5X with pressurization system to avoid chemical vapor to get inside enclosure.
Was this helpful?
What can we do to improve the information ?