Technical FAQs

Ask a Question

What are the Temperature Ranges/Conditions for ATV610 Drive ?

Below are the Temperature Conditions for ATV610 Drive.
ATV610••••• products
Frame sizes 1...6
Storage Temperature °C:-  -40...70
Temperature without derating °C :- -15...45
Temperature with derating of output power °C :- Up to 60
Temperature with derating of output power and control without Graphic display terminal °C Up to 70
at Relative humidity % 5...95
Was this helpful?
What can we do to improve the information ?