Technical FAQs

Ask a Question

What are the characteristics of external trip inputs of VIP410 protection relays.

The VIP410 has an external trip input. This input is designed to be connected to a volt-free contact (dry contact). If operation of the external trip input is enabled in the relay configuration, this contact closing will trip the circuit breaker.

Characteristics of the external contact:

Was this helpful?
What can we do to improve the information ?