Technical FAQs

Ask a Question

What is the Acceptable tolerance of the resistance at 25 deg C for DA1TT150.

The IEC 60034-11 Mark A define a single PTC sensor must have at 25°C a value between 20 Ohms and 250 Ohms.
In case the value of resistance is beyond the range mentioned then the probes needs to be tested for healthiness.
Was this helpful?
What can we do to improve the information ?