Technical FAQs

Ask a Question

What is the firmware version of CPU and CRP should be maintained if using BMXCRA in a Quantum Ethernet IO architecture.

If you use your BMXCRA in a Quantum Ethernet IO architecture, take care to update the Quantum CPU and the 140CRP31200 to the following minimum versions: 
CPU: V3.1 or higher
CRP: V1.56  or higher
Was this helpful?
What can we do to improve the information ?