Technical FAQs

Ask a Question

What if Network status LED is OFF in PDU AP7921B ?



One of the following situations exists:

• The Rack PDU is not receiving input power.

• The Rack PDU is not operating properly. It may need to be repaired or replaced. Contact Customer Support
Was this helpful?
What can we do to improve the information ?