Technical FAQs

Ask a Question

No Light indication from 10/100 LED In PDU AP7921B ?

One or more of the following situations exists:
• The Rack PDU is not receiving input power.
• The cable that connects the Rack PDU to the network is disconnected or defective
• The device that connects the Rack PDU to the network is turned off.
• The Rack PDU itself is not operating properly. It may need to be repaired or replaced. Contact Customer Support.
Was this helpful?
What can we do to improve the information ?