Technical FAQs

Ask a Question

How to write values in EEPROM parameters of Somachine HVAC controllers?

sysWritePar*() have to be used to write the EEPROM parameter in the following manner

bret := sysWriteParInt(ADR(ioEE_base_DO_05),ioSV_base_DO_05);

where ioEE_base_DO_05 is an EEprom parameter and ioSV_base_DO_05 is the variable containing the new value to be written.

Refer the attached image for example:




 
Was this helpful?
What can we do to improve the information ?