Technical FAQs

Ask a Question

How can a custom INI file be backed up along with Project backup.

If you are using a custom INI file that is stored in a sub-directory of the project, select the Save sub-directories option to back it up as well along with Project backup.
Was this helpful?
What can we do to improve the information ?