Technical FAQs

Ask a Question

At which DC bus voltage DBR (Dynamic Braking Resistor) triggers in Lexium 32 drives

Braking resistor switch on voltage is fixed by hardware and it is not configurable in LXM32.
For LXM32___M2 range threshold is 430 vdc if parameter DCbus_compat  = 0 (default) and 395 vdc if parameter DCbus_compat = 1
For LXM32___N4 range threshold is 780 vdc irrespective of parameter DCbus_compat settings.

 
Was this helpful?
What can we do to improve the information ?