Technical FAQs

Ask a Question

How many cables per phase can be installed on Ringmaster

Ringmaster C (RN2c, RE2c and RN6c)
Up to 2 cables per phase can terminated on Ringmaster C units. Special ECON cable termination kits must be used and are available from Schneider Electric

Ringmaster Range (CE2, CE6, CN2, SE6,
Only 1 cable per phase can be terminated on Ringmaster Range units.

Full installation details including cable connection is detailed in the Ringmaster Installation, operation and maintenance instructions (Ref. SE 6251) available from Schneider Electric
Was this helpful?
What can we do to improve the information ?