Technical FAQs

Ask a Question

Which "Symbol database" file types should be used with OFS for Unity Premium PLCs?

When using Aliases in OFS, pointing to a Unity Premium PLC, only two types of "Symbol database" file can be used: either user files (.STU), or project symbol export files (.XVM)"
Was this helpful?
What can we do to improve the information ?