Technical FAQs

Ask a Question

Where are pilot wire/LV cable gland holes on Ringmaster

The gland holes are located at the back of the LV compartment. There are plastic removable plugs on the Ringmaster C and knock-outs on Ringmaster Range.
Ringmaster C
Glands holes shown from inside the LV box
Gland holes shown from inside the LV box

Gland holes from underneath the LV box
Gland holes shown from underneath the LV box

Ringmaster Range
Gland holes from inside the LV box
Gland holes shown from inside the LV box

Gland holes from underneath the LV box
Gland holes shown from underneath the LV box
 
Was this helpful?
What can we do to improve the information ?