Technical FAQs

Ask a Question

In which configuration can I install a 140ESI06210 card?

The 140ESI06210 card can be installed on a local, decentralised or remote Quantum sub-base. However the card's firmware can only be downloaded to a local sub-base. It may therefore be sensible to leave a slot on the local sub-base empty to update any card that is installed on a decentralised or remote sub-base.
Was this helpful?
What can we do to improve the information ?