Technical FAQs

Ask a Question

What is the consumption of a Modicon Micro PLC on 24 VDC?

 Expect 1.25 A max. in transient state, and 0.8 A at maximum continuous current, on 24 VDC. These characteristics apply to all 24 VDC models in the Modicon Micro range.  Example: 110CPU61200 or 110CPU31103. 
Was this helpful?
What can we do to improve the information ?