Technical FAQs

Ask a Question

How can I start counting on the high speed counter 140EHC10500 without using the validation input?

 In Concept 2.11, to start counting without using the input corresponding to the channel being used, which is generally used as a validation input, simply do not check the line "Use counting enable input x" and do not declare anything next to the "Input A" line. The control panel of the 140EHC10500 high speed counter card can be accessed from the "Local Quantum I/O Station" screen in which the "Parameters" button is located. This button is operational when the line is highlighted.
Was this helpful?
What can we do to improve the information ?