Technical FAQs

Ask a Question

How many samples per cycle are captured for the Sepam Series 20, 40 and 80? How many samples are used for protection, measurement, and waveform display?

The Sepam protection relay samples at 36 samples per cycle to calculate true RMS values for displayed phase current and overload protection. It can analyzes up to the 17th harmonic. All other measurements and protection values are calculated from the fundamental RMS calculation. The fault recording displays (waveform capture) only 12 samples per cycle for the Series 20 and 40. The Series 80 relay has an additional option of choosing 36 samples per cycle. Fault recording can be configured using SFT2841:

Was this helpful?
What can we do to improve the information ?