Technical FAQs

Ask a Question

Which is the latest Premium Hot standby PLC firmware available

Since the launch of the system Premium Hot standby PLC has only one firmware available i.e. Version 2.5.

Though we have higher versions 2.6 & 2.7 available to be selected in Unity 4.1, one has to select the correct firmware version 2.5.
Was this helpful?
What can we do to improve the information ?